How do you customize Part Name or DB_PART_NAME for the title bar in graphics window

2019-06-04T16:24:21Z

Summary


Details

--------------- 
By default, the title bar of the graphics window uses $FILENAME. So it uses the 
part file name in the operating system in native NX when you create 
your file. Can you customize the title bar of the graphics window?



Solution

 This is controlled by a customer default called "Part Name Style Attribute". 
This field allows a part attribute title to be entered. The value of this 
attribute will be displayed in dialog boxes and the graphics window title bar. 
Valid options include $FILENAME, $DESCRIPTION, and anything else deemed to 
be a part attribute title.


In the customer Default under Assemblies --> General --> Miscellaneous --> 
Part Name Style Attribute --> Enter system part attribute or user defined 
attribute title you wish.


If you run NXMGR, DB_PART_NAME could be entered.


Note that only a single attribute can be entered for this value.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V12.0.2
Function: PART_FILE_OPS

Ref: 001-8954038

KB Article ID# PL8010098

Contents

SummaryDetails

Associated Components