How to delete an Isolate Model View

2019-05-15T16:43:23Z

Summary


Details

In the Assembly Navigator, by performing a 'MouseButton3 (MB3) --> Isolate in 
New Window' operation, NX created a new Model View titled: Isolate 
How can the 'Isolate' Model View be deleted? 
When attempting to delete the 'Isolate' Model View, the following message is 
displayed: 
 A view currently in a layout may not be deleted



Solution

 Once the 'Isolate' Model View is created, it is used by the current Layout. Any 
view used in a Layout cannot be deleted.


However, the 'Isolate' view is only a temporary view for the NX session. 
1. Save the part without saving the Layout. 
 A. 'File-->Save-->Save'. 
2. Close the Part. 
 A. 'File-->Close-->All Parts'. 
3. Re-open the part. 
 A. 'File-->Open' and select the part file to open. 
In the Part Navigator, the 'Isolate' Model View will no longer be in the list 
of Model Views.


If it is not possible to save, close, and re-open the file, then the following 
can be used to delete the 'Isolate' Model View: 
1. Save the current Layout without using the 'Isolate' Model View. 
 A. In the Part Navigator under 'Model Views', make sure the 'Isolate' 
 Model View is NOT the current "(Work)" view. 
 B. In the Menu, select 'View-->Layout-->Save'. 
2. Open a different Layout. 
 A. In the Menu, select 'View-->Layout-->Open'. 
 B. Select the Layout, 'L2 - side by side'. 
 C. OK the Open Layout dialog. 
3. Delete the 'Isolate' Model View. 
 A. In the Part Navigator, select the 'Isolate' Model View, 'MB3-->Delete'. 
4. Switch back to the Single View Layout. 
 A. In the Menu, select 'View-->Layout-->Open'. 
 B. Select the Layout, 'L1 - single view'. 
 C. OK the Open Layout dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V11.0.1
Function: FEATURE_MODEL

Ref: 001-7998995

KB Article ID# PL8010084

Contents

SummaryDetails

Associated Components