Renaming part versions during a Clone operation

2019-05-15T16:39:59Z

Summary


Details

When importing an assembly that contains multiple revisions of the same part, 
the import is creating two separate parts in Teamcenter.


For example, when importing an assembly (using Auto Translate), that contains 
a revision A and B of the same part, only revision A is imported correctly. 
Revision B is imported using Auto Generate and given a new number.


Parts included in import: 
ABCDE_001.prt 
ABCDE_002.prt


The parts are imported as: 
@DB/ABCDE/001 
@DB/0011/001



Solution

 If subsequent revisions are imported using Auto Generate instead of Auto 
Translate when the 'Enable Multiple Revisions' option is toggled off. 
Please toggle on 'Enable Multiple Revisions' in Customer Defaults. 
1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Teamcenter Integration for NX' and highlight 'General'. 
3. Select the 'Multiple Revisions' tab. 
4. Toggle ON 'Enable Multiple Revisions'. 
5. OK the Customer Defaults dialog. 
6. Re-start NX.


Once 'Enable Multiple Revisions' is toggled on, the import of both parts is 
successful using Auto Translate. 
@DB/ABCDE/001 
@DB/ABCDE/002



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V9.0
Function: CLONE_IMPORT

Ref: 001-7188938

KB Article ID# PL8010066

Contents

SummaryDetails

Associated Components