Hidden Tapered threads showing in drawing view

2019-05-15T16:42:47Z

Summary


Details

Tapered threads appear in a drawing view, even though they are hidden and the 
Hidden Line Font is set to 'Invisible'.



Solution

 1. Hover the cursor over the view, 'MouseButton3-->Style'. 
2. Select the 'Threads' tab. 
3. Toggle ON, 'Render True Hidden Line'. 
4. OK the View Style dialog.


The 'Render True Hidden Line' option increases the quality of the rendered 
thread so more atypical threads are correctly rendered. This increases the 
quality so that incorrectly trimmed thread lines appear correctly. With this 
option set, the time to display the view may increase when there are numerous 
threads.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.5.3
Function: DRAWING/VIEW

Ref: 001-7749139

KB Article ID# PL8010065

Contents

SummaryDetails

Associated Components