Part is non_geom despite of TC_NX_Unit_Of_Measure_As_Geometric_List

2019-05-08T09:44:19Z

Summary


Details

--------------- 
SOFTWARE VERSIONS 
=================== 
TC 10.1.* and higher
NX 10.0.* and higher


PROBLEM DESCRIPTION 
===================== 
We have a component , which has custom unit of measure. 
We set TC_NX_Unit_Of_Measure_As_Geometric_List=* to have ability to add 
component , which has custom unit of measure as geometric. 
When we add such component to an assembly in Teamcenter, and open assembly in 
NX, the component is added as non-geometric.


TC_NX_Unit_Of_Measure_As_Geometric_List is ignored.


STEPS TO REPRODUCE 
==================== 
  • Open TC\Structure Manager app. 
  • Create structure (assembly) from 2 components: first component has standard unit of measure, second component has custom unit of measure. 
  • Open assembly in NX. 
Can see: first component can be added from "Pending components" and we have a 
choice . 
But second component is added at once as non-geom. 
____________________________


Reference: PR#8319610





Solution

Works as designed: TC_NX_Unit_Of_Measure_As_Geometric_List is only NX preference.
I.e. only components, which are created in NX, account this preference.

Documentation of NX12 are updated. TC_NX_Unit_Of_Measure_As_Geometric_List preference description contains the following details:
"This preference is only applicable when you create components in NX. If you create components in Teamcenter, this preference is ignored." 

WORKAROUNDS 
==============


1) To add a component (which has a custom unit) using NX commands.


2) If we added such component from TC, we can edit component properties in NX: 
tun off "non-geometric" checkmark.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2016
Product: NX
Application: NXMANAGER
Version: V12.0
Function: PREFERENCES

Ref: 001-8319610

KB Article ID# PL8010062

Contents

SummaryDetails

Associated Components