Cannot change Title Block cell SH_PART_NAME to DB_PART_NO

2019-08-28T14:57:56Z

Summary


Details

--------------- 
A user is attempting to edit a part file that is used as a template. In the 
Title Block, the attribute that is being used for the "Model Name" is 
"W@$SH_PART_NAME". Using that attribute while in Teamcenter will add the 
Revision to the end of the name, i.e "A-Size/A", customer wants the name but 
no revision. 


When attempting to edit the Title Block using "Edit Definition" the cells are 
locked and can not be unlocked. How do you change the attribute?



Solution

 The Lock symbol that display is a "lock w/screwdriver", and this indicates that
it is an Automatic Lock and can not be unlocked. This happens when a cell 
contains more than one attribute, expression, or other object.


To change the Attribute, the Table needs to be removed from the Title Block. 


To do this, edit the Title Block by selecting the Title Block --> MB3 --> Edit 
Definition. Then select and highlight the "Tables" section of the dialog and 
use 'Shift+Select' to deselect the table that contains the cell you need to 
edit --> OK. Now that the Table is removed from the Title Block, you will be 
able to double click in the cell and edit the text string; 


 From: <C2.500><W@$SH_PART_NAME><C>" 
 To: <C2.500><W@DB_PART_NO><C>


Select [Enter] to complete the edit.


To re-Add the table back to the Title Block, select the Title Block and 
use "Edit Definition" again. Select and highlight the "Tables" section of 
the dialog and select the Table that was edited. Select OK to complete the 
edit.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.5
Function: DRAWING/VIEW

Ref: 001-6924340

KB Article ID# PL8010046

Contents

SummaryDetails

Associated Components