How to Determine if a User is Using Ribbon or Classic Layout

2019-04-25T11:56:52Z

Summary


Details

How to determine if a user is using the Ribbon or Classic Layout in NX9 and 
higher.



Solution

 In the user.mtx file towards the bottom of the file, you will find either one 
of these settings.


Ribbon Bar Settings:


 <SessionSettings>
 <Setting name="RibbonMinimized" ribbonMinimized="0"
ribbonFullscreenMinimized="0"/>
 <Setting name="UserInterfaceMode" defaultModeSetup="1"/>


OR


Classic Settings:


 <SessionSettings>
 <Setting name="RibbonMinimized" ribbonMinimized="0"
ribbonFullscreenMinimized="0"/>
 <Setting name="UserInterfaceMode" defaultModeSetup="0"/>


Notice the "<Setting name="UserInterfaceMode" defaultModeSetup="1"/>" is :

1 for Ribbon and ,

0 for Classic



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V1847
Function: UI_TOOLS

Ref: 001-7640954

KB Article ID# PL8010032

Contents

SummaryDetails

Associated Components