Creating a Spine/Curve from points in a CSV file

2019-04-29T18:30:42Z

Summary


Details

--------------- 
Is there a way to read in a Comma Seperated Values (CSV) file & create a curve 
thru these points? Is there also a way to include the points?



Solution

 You can import the points using File --> Import --> Points From File.


You can create a spline using Insert --> Curve --> Spline (you may need to add 
this option to the menu via Tools --> Customize) --> Thru Points button --> 
Points From File. This will create a spline and then you can use Insert --> 
Datum/Point --> Point Set --> Type = Spline Points to recreate the points.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1847
Function: CURVE

Ref: 001-7203002

KB Article ID# PL8010030

Contents

SummaryDetails

Associated Components