Weight in the Assembly Navigator differs from Measure Bodies

2019-05-15T15:27:53Z

Summary


Details

On single parts, the Weight value displayed in the Assembly Navigator 
differs from the Weight value given by the 'Measure Bodies' command.



Solution

 The Assembly Navigator weight value is based on the Reference Set specified in 
the 'Analysis-->Advanced Mass Properties-->Advanced Weight Management' command.


In 'Advanced Weight Management', if the Reference Set is set to 'Entire Part', 
the entire part is used in the weight calculations. This could result in 
inaccurate weights for parts with more than one body (for example, sheetmetal 
parts with a flat solid).


Verify that only the body needed for the weight calculation is in a specified 
reference set. Then in 'Advanced Weight Management', use this reference set. 


When 'Weight' is updated in the part's Properties, the Assembly Navigator 
should display the weight for only those bodies used in the specified reference 
set.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V8.5
Function: ASSEMBLY_MODEL

Ref: 001-7148566

KB Article ID# PL8010029

Contents

SummaryDetails

Associated Components