Assembly Navigator is stuck off-screen

2019-05-15T16:38:38Z

Summary


Details

How to correct the Assembly Navigator position when the Assembly Navigator is 
undocked and stuck off-screen.



Solution

 In the Menu, select 'Tools-->Assembly Navigator-->Exit'. 
This will bring the Assembly Navigator back to the Resource Bar as a tab. 
However when it the Assembly Navigator is undocked again, it will again go 
off-screen.


The Navigator positions are stored by application (Modeling, Drafting, 
Gateway, Manufacturing, etc.). 
For example, if this is an issue in the Modeling application, go to regedit and 
delete the Navigator folder under "Modeling" (UG_APP_MODELING). 
1. Exit NX. 
2. Start regedit. 
3. Browse to the following location: 
 HKEY_CURRENT_USER\Software\Unigraphics Solutions\NX\9.0 
 \Layout\Applications\UG_APP_MODELING 
4. Highlight the 'Navigators' folder in this location, 
 'MouseButton3-->Delete'. 
5. Exit regedit. 
6. Re-start NX. 
The Navigator positions for Modeling should now be back to the out-of-the-box 
position.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V9.0
Function: NAVIGATORS

Ref: 001-7492214

KB Article ID# PL8010026

Contents

SummaryDetails

Associated Components