---------------
Occasionally you might find it necessary to add some additional reference text notes to sketch dimensions in the form of appended text.
Solution
To add a note as text appended to a sketch dimension perform the following steps:
o Select a sketch dimension after it is created
o Use MB3-> Edit...
o Toggle ON Enable Dimension Scene Dialogs to activate appended text editor access on dimension

o Select the "Text" icon on the dimension dialog to enter the Text Editor

o Select the Edit Appended Text icon to activate that dialog

o Select the desired Text Location from the drop down list
o Enter the text in the Text Input area

o Close all the dialogs to apply the appended text
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1847
Function: SKETCHER
Ref: 001-6858085