NX Check-Mate results are not displayed in HD3D tools dialog when tests are run.

2019-05-20T15:30:37Z
NX for Design

Summary


Details

--------------- 
When running Check-Mate tests on a part no results are displayed in the HD3D Tools Check-mate navigator.



Solution

 Ensure that the following setting is unchecked in the Check-Mate navigator :


"Show Overridden Only"

If this is ON nothing will be displayed for a new test run. 


Note - This dialog uses dialog memory control so it will remember the last settings used in this session or the last session it was accessed.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: KDA
Version: V1847
Function: VALIDATION

Ref: 001-7184607

KB Article ID# PL8010013

Contents

SummaryDetails

Associated Components

Modeling