Setting a default directory for load options

2019-04-29T17:05:23Z

Summary


Details

--------------- 
How can you point to a custom load options file?



Solution

 Set UGII_LOAD_OPTIONS to point to the desired directory and file.


This variable defines the ascii file that contains the load options settings. 
If it is not set, a file called load_options.def in the current directory is 
searched for instead. NOTE: If you set this to a file specification that 
contains spaces, you must enclose the file in quotes, e.g


UGII_LOAD_OPTIONS="c:\my Data Files\load_options.def"



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V1847
Function: PART_FILE_OPS

Ref: 001-6871440

KB Article ID# PL8009987

Contents

SummaryDetails

Associated Components