NX What PCB Exchange .ini file stores the Component Load Options?

2019-05-15T16:34:47Z
NX for Design

Summary


Details

In NX9, in the PCB Exchange settings ('PCA' tab), there are now 3 options for 
the "Component Load Options". 
-Load and Create Assembly Components 
-Create Bodies Only 
-Load Assembly Components, Create Bodies 
How to set one of these three options in an .ini file?



Solution

 This setting needs to be added (not currently listed). 
The Component Load Options can be controlled by adding the following setting to 
the %UGII_BASE_DIR%\UGPCBXCHANGE\pcbx_ug_model.ini file: 
 NXWriteComponentAs


Use one of the following values: 
- ComponentsOnly 
- BodiesOnly 
- LoadComponentsCreateBodies


For example: 
NXWriteComponentAs = BodiesOnly



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: PCB_EXCHANGE
Version: V9.0
Function: ALL

Ref: 001-7163559

KB Article ID# PL8009964

Contents

SummaryDetails

Associated Components

PCB Design