altering the number of decimal places displayed in Tool Path Verifiy

2019-05-15T15:25:49Z

Summary


Details

When performing a tool path verification, the coordinates shown at the top of the verify dialog are using three decimal places.  Is it possible to change this and show more decimal places?

Solution

Yes. In the NX session, go to:

File; Utilities; Customer Defaults 

-- Manufacturing 

----Simulation & Visualization 

------ General tab 

-------- there is a Decimal Places slider bar at the bottom of the tab to control the number of decimal places displayed

Note that NX will need to be restarted for this change to take effect.

Notes

KB Article ID# PL8009942

Contents

SummaryDetails

Associated Components