Getting rid of external references when importing assembly to Teamcenter

2019-05-30T18:09:53Z

Summary


Details

--------------- 
Sometimes during the import of an assembly to TC, there are some external 
referenced files that are not physically in the assembly but could cause 
problems on import. You can usually find out about these references after 
adding an assembly to import, then go to --> Numbering tab --> Exceptions. The 
references would be listed as: "file name" (Default)(Name Only). 
How do you get rid of these references?



Solution

 One way that you can remove these dead external references before import is to 
open the assembly fully, (Partial Load toggled off from Assembly Load Options), 
then --> Information --> Part --> Loaded Parts and you can see the referenced 
parts listed at the bottom as:


"file name.prt" "file name" Not Loaded.


If they are really dead references, then you can do Part Cleanup turning all 
switches except the serious delete action. Now try Information --> Part -> 
Loaded Parts again and the referenced parts should be gone.


Note that while these part cleanup tools are very useful, they do not cover all 
possible data scenarios or all possible application specific constructs. For 
example, unresolved inter-part references are not identified and cleaned. And 
one reason for not doing this is that tools should not remove information the 
user may potentially want to use at some later point in time. For example, the 
user will not be able to delete component array references if the master array 
has not been deleted, since some users might want the ability to re-associate 
to references later. Therefore, to really delete the unwanted reference, the 
user would need to manually go to the Edit Component Arrays dialog ( Assemblies 
--> Component --> Edit Component Array) and then delete the arrays that are no 
longer valid (or unsuppress them and pick delete).


What causes these external references to show up in the assembly?


NX has the ability to create interpart references in many different ways 
throughout an assembly. They can be done using Part Families, WAVE links, 
Interpart expressions, Promotions and Positioning Constraints to mention a few.


When parts are not managed by a robust PDM system like Teamcenter it is very 
easy to delete a (place holder) part not knowing that it is used by an 
assembly, or by another part. This is the most common reason for cases 
of dead references. Other known issues are users renaming parts on the OS; 
the name seen by the user looks correct after the rename, however, any part 
referencing the renamed part is in fact referencing its internal name, 
which was not renamed. 


In this scenario ug_clone could potentially now be looking for two references 
of the same part - of course when searching the OS you'll never find the 
original part because it was renamed.


As for avoiding these issues in the future, Teamcenter will help tremendously 
by preventing users from deleting referenced parts.


It should also be noted that the Teamcenter import utility does allow the 
importing of assemblies that contain references to data that are not contained 
in the assembly. These are treated as "Name Only" references and thus do not 
require the importing of the missing referenced data. Also, customers that 
need customer-specific cleanup capability have the option to write their own JA 
or NX/Open type automation utility.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: CLONE_IMPORT

Ref: 001-7275272

KB Article ID# PL8009939

Contents

SummaryDetails

Associated Components