A Linear dimension arrow has no tail when set to 'Arrows Out'

2019-12-23T08:44:03Z

Summary


Details

When a linear dimension is created with the arrows positioned outside of the extension lines (Arrows Out), the arrow on the opposite side to the dimension value has a head, but no tail.


Solution

On a Linear 'Arrows Out' dimension, the length of the arrowhead tail of the arrow opposite the dimension text, is a factor of the dimension text height. Therefore, reducing the text height shortens the arrow tail length, which can result in no tail being displayed at all.

There is currently no way to modify this for existing dimensions, as there is no option to change the 'Dimension Arrow Out Length Factor' value via the dimension 'Settings' dialog. An enhancement request (ER 1961494) has been submitted to address this.

In the meantime, the workaround is to modify the value of the 'Dimension Arrow Out Length Factor' in the Customer Defaults, and apply that change to the drawing, so that new 'Arrows Out' dimensions will have a tail.

The procedure to workaround this issue is as follows:


1. Select 'File -> Utilities -> Customer Defaults -> Drafting -> General/Setup -> Standard (tab) -> Customize Standard' then select 'Common -> Line/Arrow -> Arrowhead (tab)' and set the value for 'Dimension Arrow Out Length Factor'. (The default value in '2.5'.)


2. Use 'Save' (or 'Save As') to update the Drafting Standards.


3. Restart NX and open the drawing that has this dimension appearance problem.


4. Select 'Menu -> Tools -> Drafting Standard...' choose the modified standard and select 'OK'.


5. Create a new dimension with 'Arrows Out' and both arrows will have a tail.


Note: Existing dimension cannot be modified, new dimensions must be created.

Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V12.0
Function: DIMENSION

Ref: 001-7687244

KB Article ID# PL8009935

Contents

SummaryDetails

Associated Components