Creating a point coordinate note in Drafting

2019-04-26T13:40:54Z

Summary


Details

--------------- 
How can you create a point coordinate note in Drafting?



Solution

 In Modeling, PMI --> Specialized --> Coordinate Note.


Once the Note is created, you can display the Note in Drafting by toggling on 
Aligned to View or Aligned to Drawing under Common --> PMI of the View Settings dialog.

You must create a Draft view that is the same as the view the Note was created 
in or the note will not be visible (view dependent).

However, you can set Display in All Views for PMI by selecting Prefereces --> 
PMI --> toggle on Display in all Views under the Creation Options section.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1847
Function: DRAWING/VIEW

Ref: 001-6963604

KB Article ID# PL8009930

Contents

SummaryDetails

Associated Components