NX Error in inxInitialize when trying to migrate data using CMM on a machine.

2019-05-13T15:00:35Z
NX Design Translators

Summary


Details

Receiving the following error in the CMM log file whe attempting to migrate 
data inside TC:


*** 2017-01-27 10:48:53.918 Critical Error : java.io.IOException: Error in 
inxInitialize 
 
com.ugsolutions.ideasnxmigration.migrationmanager.util.helper.CMMException: 
Fatal Error ! 
 at 
com.ugsolutions.ideasnxmigration.migrationmanager.framework.migrationcontrol.Se 
rviceBroker.startIDEASService(ServiceBroker.java:176) 
 at 
com.ugsolutions.ideasnxmigration.migrationmanager.framework.migrationcontrol.Mi 
grationControl.validateIdeasPart(MigrationControl.java:5418) 
 at 
com.ugsolutions.ideasnxmigration.migrationmanager.framework.migrationcontrol.Mi 
grationControl.processElement(MigrationControl.java:3173) 
 at 
com.ugsolutions.ideasnxmigration.migrationmanager.framework.migrationcontrol.Mi 
grationControl.execute(MigrationControl.java:1035) 
 at 
com.ugsolutions.ideasnxmigration.migrationmanager.framework.migrationcontrol.Th 
readedMigrationControl.run(ThreadedMigrationControl.java:33) 
 at java.lang.Thread.run(Thread.java:744)


The ideasservice.log file shows the following:


 ERROR>Fatal error: No shared object found 
*** Client: Unable to read from socket 
*** Server not responding 
*** Error in sendMessage 
*** Error in inxInitialize 
*** Client: Unable to read from socket 
*** Server not responding 
*** Error in sendMessage 
*** Error in inxClose 
 Terminating process ...



Solution

CMM was installed in the Program Files directory. The spaces in the file 
directory structure make trouble for I-deas so the solution was to uninstall 
CMM from the Program Files directory and to install it into a short filename 
directory without spaces.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CMM
Version: V10.0.3
Function: INSTALL

Ref: 001-7939486

KB Article ID# PL8009929

Contents

SummaryDetails

Associated Components

Content Migration Manager