How can I prevent the "Check Mate Result" and other pop-up dialog's from becoming nearly
translucent or transparent when the cursor is not over them?
Solution
Users can turn off "Windows" transparency. Disabling transparency affects all windows in NX and displays them as opaque when the cursor is not immediately over them.
The old "Legacy" interface requires users to select, 'Preferences -> User Interface -> (tab) Layout -> (uncheck the box) Enable Transparency.'


The new "Ribbon Bar" interface requires users to select, 'File -> Preferences -> User Interface -> Theme -> Transparency -> (uncheck the box) Enable Transparency for UI Components.'


Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 10_1507
Product: NX
Application: GATEWAY
Version: V1859
Function: PREFERENCES
Ref: 001-6740782