How to use 'Mark as Template and Update PAX File'

2019-05-15T15:25:09Z

Summary


Details

A new drawing template file created using the 'Tools-->Drawing Format-->Mark as 
Template' command is not saving in the correct location.



Solution

 1. When saving new drawing templates using 'Tools-->Drawing Format-->Mark as 
Template' and selecting the 'Mark as Template and Update PAX File' option, make 
sure to select the correct PAX file using the Browse command. 
2. Save the drawing template file in the same directory as the existing PAX 
file. Typically this is in the %UGII_BASE_DIR%\UGII\TEMPLATES directory.


NOTE: The template file needs to be in the same directory as the PAX file. 
If the template file is in an alternate location, the directory path must be 
used in the PAX file to completely define the template's location.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.0
Function: TABLES

Ref: 001-6712007

KB Article ID# PL8009906

Contents

SummaryDetails

Associated Components