The 'Face Option' is missing on the dialog when WAVE Linking a face

2019-05-15T16:32:05Z

Summary


Details

The 'Face Option' on the WAVE Geometry Linker dialog is missing. 
For example: 
1. Select 'Insert-->Associative Copy-->WAVE Geometry Linker'. 
2. Set 'Type = Face'. 
Notice that the 'Face Option' is missing under the Face group in the dialog.



Solution

 This is a Customer Default option. 
1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Modeling' and highlight 'Feature Parameters'. 
3. Select the 'Extract and WAVE Geometry Linker' tab. 
4. Toggle ON 'Enable Legacy 'Face option' Menu'. 
5. OK the Customer Defaults dialog. 
6. Restart NX.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V9.0
Function: WAVE

Ref: 001-6981336

KB Article ID# PL8009890

Contents

SummaryDetails

Associated Components