In the Drafting application only the model can be seen

2019-05-15T16:31:21Z

Summary


Details

In the Drafting application, only the 3D model is seen. The View creation 
commands are grayed out and the 'Display Sheet' icon is also grayed out and 
unavailable for selection.



Solution

 It could be that there are no sheets in the drawing. 
In the Part Navigator, expand 'Drawing'. 
If there are no sheets listed under the Drawing, then the view creation icons 
and the 'Display Sheet' icon will be grayed out. 
1. In the Part Navigator, highlight 'Drawing'. 
2. 'MouseButton3-->Insert Sheet'. 
3. Set the desired sheet settings. 
4. OK the Sheet dialog. 
Now the view creation icons should no longer be grayed out and the 'Display 
Sheet' command should become available.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.5
Function: DRAWING/VIEW

Ref: 001-7151580

KB Article ID# PL8009886

Contents

SummaryDetails

Associated Components