---------------
After adding a View Break with the Style set to Solid Tubular, the
crosshatching is placed on the inside of the tube face, when it should
be on cut face of the tube. How do you reverse it?
Solution
One reason may be that the Amplitude setting is to small. The crosshatch
can be reversed by changing the Amplitude setting to a larger size, if it is
set to 0.30, change it to 0.50 and adjust accordingly.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V10.0
Function: DRAWING/VIEW
Ref: 001-7562759