Stacking does not work after annotation is created

2019-05-15T16:29:45Z

Summary


Details

The stacking functionality in Annotation is working upon creation of the 
annotation; however editing existing annotation to stack does not show any of 
the stacking alignment icons. Existing annotation cannot be stacked.


For example: 
1. In NX, in the Drafting application, create two separate Notes on a drawing. 
2. After the Notes have been created, drag one Note to stack it into the 
 other. 
 Stacking symbols should appear to allow the second Note to be stacked into 
 the first Note. 
However, no dashed boxes or stacking symbols are appearing allowing the Notes 
to be stacked together.



Solution

 1. In the Menu, select 'Preferences-->Drafting'. 
2. Expand 'Common' and highlight 'Workflow'. 
3. Toggle on 'Dynamic Alignment in Global Selection'. 
4. OK the Drafting Preferences dialog.


Now when dragging existing annotation to stack with other annotation, the 
stacking icons and dashed boxes will appear to allow stacking.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.5
Function: ANNOTATION

Ref: 001-7245551

KB Article ID# PL8009869

Contents

SummaryDetails

Associated Components