How to align a drafting view with a point on the drawing sheet

2019-05-21T13:37:30Z

Summary


Details

The 'View Alignment' command cannot be used to align an existing view to a point on the sheet. When using the 'Placement Method - Horizontal' and the 'Alignment' option is set to 'Point to Point', it is not possible to select a point on the sheet as the 'Stationary View Point'.



Solution

 Use the view 'Edit' command to align the view to a point on the sheet.


1. Place the cursor on the boundary of the view to be aligned to the point and select the right-hand mouse button menu option 'Edit'.


2. Set the 'Placement - Method' to 'Horizontal' (or 'Vertical') and 'Alignment' to 'Point to Point'. (Ensure that the Snap Point selection filter has 'Existing Point' selected.) Deselect the 'Associative Alignment' option. Select the point on the sheet as the 'Stationary View Point' and a point in the view as the 'Current View Point'.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V12.0
Function: DRAWING/VIEW

Ref: 001-7272548

KB Article ID# PL8009866

Contents

SummaryDetails

Associated Components