NX NX CAM - Change Direction of a STEP2HOLE Feature

2019-10-18T06:53:57Z
NX for Manufacturing

Summary


Details

--------------- 

Problem with 'flip direction' of a non-symmetrical features such as STEP2HOLE:

'MB3 - flip direction' is available , but has no effect.

Solution

'Flip direction' of non-symmetrical features such as STEP2HOLE is not implemented

Workaround is to manually edit - with "Edit Feature CSYS".

Notes

ER 7719572

KB Article ID# PL8009863

Contents

SummaryDetails

Associated Components

Manufacturing General