In the Lightweight Section View dialog, the 'Section Name' is grayed out and
unable to be modified. Also, if the Lightweight Section View is created, there
is no 'Rename' option under MouseButton3 in the Part Navigator.
How can the Section Name be changed?
Solution
Under the 'Cutting Plane' Symbol group in the Lightweight Section View dialog,
if 'View Name Format' is set to a either 'A' or 'A-A', this controls the naming
format of the view and can only be altered by specifying the 'Text' such as
A,B, C, D. Once one of these options is used to name the Lightweight Section
View, the view will NOT have a 'Rename' option under MouseButton3 in the Part
Navigator.
Under the 'Cutting Plane' Symbol group in the Lightweight Section View dialog,
if the 'View Name Format' is set to 'User Defined', the Section Name
can be set as desired. This also allows the 'MB3-->Rename' option to appear in
the Part Navigator since the name of the view has been set to 'User Defined'.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: PMI
Version: V9.0
Function: SECT_VIEW_LGCY
Ref: 001-7187455