How to extract image files inserted in to an NX Drawing?

2019-07-29T08:50:51Z

Summary


Details

Image files inserted in to an NX drawing (via 'Menu -> Insert -> Image') cannot be subsequently extracted. (They can be deleted, but then the image is lost.)

Solution

A workaround to this issue is to use '7-zip' to open the drawing '.prt' file as an archive file. This will expose the internal structure of the drawing file, the images are stored in the 'drafting -> images' folder.

To extract the image file, select it and use the right-hand mouse button option 'Copy to...' and specify the designation folder.

The exported file can be renamed to add the appropriate file extension, for example '.jpg'.


Warning! : Editing an NX part file in this manner has the potential to cause data corruption, only perform this operation on a copy of the NX .prt file.

Note: This workaround only applies up to and including NX 11. An NX 12 '.prt' cannot be opened as a archive file using 7-zip.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V11.0
Function: ANNOTATION

Ref: 001-8320480

KB Article ID# PL8009855

Contents

SummaryDetails

Associated Components