Where is "From Point Cloud" in NX 9 and later?

2019-04-25T20:18:48Z

Summary


Details

--------------- 
What happened to the surface function "From Point Cloud" in NX 8.5 and higher?



Solution

 This function was removed in NX 8.5 and replaced with Fit Surface.


The functionality may appear to be different, but the end result is basically 
the same. A surface which best fits the data points selected. And there is 
additional functionality like creating not only a best fit B-surface but 
also a best fit plane, cylinder, sphere or cone and the results are 
associative in that if the points move the surface will update. And if you 
use the new NX 8.5 File -> Import -> Points from a file function the points 
will be in named groups which means that it will be easy to load-up a 
modified set of points and edit the surface by replacing one named-group of 
points with a new named-group thus allowing you to update an existing 
surface based on a new set of data points.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V9.0
Function: FREE_FORM_MODEL

Ref: 001-6991940

KB Article ID# PL8009849

Contents

SummaryDetails

Associated Components