The text "
THRU" is automatically added to Hole Callout dimensions if the selected hole feature is a through hole.

Solution
In NX 10 and NX 11, the "
THRU" text can be removed from the Hole Callout by selecting the dimension and using '
MB3 - Settings', on the '
Hole Callout' page
uncheck the '
Depth' option under '
Parameters'.

Note: If the hole feature is subsequently changed to a blind hole, the Hole Callout does not update automatically to include the depth value. The depth value will need to be enabled by checking the '
Depth' option within '
Settings'.
The only way to prevent the '
THRU' text from being added automatically is to uncheck the '
Depth' option in '
File - Utilities - Customer Defaults - Drafting - General/Setup - Standard - Customize Standard - Dimension - Hole Callout - Threaded Hole'. However, this will suppress/hide the depth information from all new Hole Callouts created after the Drafting Standard changes have been applied.
In NX 12 (and later releases), the dimension '
Settings - Hole Callout' dialog contains a '
Through Hole Text' field that allows the text to be edited or removed.

There is also a '
Through Hole Text' customer default that allows the Through Hole text to be defined (or removed). This default is located under '
File - Utilities - Customer Defaults - Drafting - General/Setup - Standard - Customize Standard - Dimension - Hole Callout - General Hole/Drill Size Hole/Screw Clearance Hole/Threaded Hole'.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V10.0
Function: DIMENSION
Ref: 001-8824471