Translucency is lost after selecting first edge

2019-05-15T16:27:13Z

Summary


Details

Selecting an edge in the 'Edge Blend' command causes the model to lose 
translucency so hidden edges cannot be selected.


For example, when a part has translucency set to 50%, and the 'Edge Blend' icon 
is selected, the edges on the backside of the part are visible and the first 
edge can be selected. However, at this point the part loses translucency and 
the remaining edges on the backside of the part are no longer visible and 
cannot easily be selected.



Solution

 This is the result of a Visualization setting. 
1. Select 'Preferences-->Visualization'. 
2. Select the 'Emphasis' tab. 
3. Toggle off 'See-Thru Preview'. 
4. OK the Visualization Preferences. 
Now the hidden edges should stay visible during the 'Edge Blend' command.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V8.5
Function: PREFERENCES

Ref: 001-6963770

KB Article ID# PL8009834

Contents

SummaryDetails

Associated Components