How to orient the WCS to the end point of a line

2019-05-15T15:23:31Z

Summary


Details

How to orient the WCS to the end point of a line.



Solution

 1. In the Menu, select 'Format-->WCS-->Orient'. 
2. Set the Type to 'Inferred'. 
3. Select the line somewhere other than the end point. 
4. Select the end point of the same line. 
The WCS will now be located at the end of the line with the Z axis 
parallel to the line. The X-Y axis will be perpendicular to the line end 
point.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V7.5.5
Function: WCS

Ref: 001-7776047

KB Article ID# PL8009821

Contents

SummaryDetails

Associated Components