How to remove material assigned to a solid body

2019-05-15T15:23:27Z

Summary


Details

How to remove a material assigned to a solid body.



Solution

 1. Select 'Tools-->Materials-->Manage Materials'. 
2. Set the Materials List to 'Local Materials'. 
3. Highlight the listed material that has a green check mark in 
 the 'Used' column. 
4. Select the 'Remove selected material assignments' icon. 
 The material assignment will be removed from the solid body; however, 
 the material will remain a local material unless the material is 
 highlighted in the list and the 'Delete selected material' icon is used. 
5. Close the Manage Materials dialog.


NOTE: The solid body will retain the density of the assigned material but this 
can be modified using the 'Edit-->Feature-->Density' command.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V9.0
Function: FEATURE_MODEL

Ref: 001-7268346

KB Article ID# PL8009820

Contents

SummaryDetails

Associated Components