'Create Interpart Link' option is grayed out in the Selection Toolbar

2019-05-15T16:26:03Z

Summary


Details

Why is the 'Create Interpart Link' option grayed out in the Selection Toolbar 
during NX commands?



Solution

 This option has to be turned on in Customer Defaults. 
1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Assemblies' and highlight 'General'. 
3. Select the 'Interpart Modeling' tab. 
4. Toggle 'Allow Associative Interpart Modeling' to 'Yes'. 
5. OK the Customer Defaults dialog. 
6. Re-start NX. 
Now the 'Create Interpart Link' option will be available within commands.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V9.0
Function: WAVE

Ref: 001-7642215

KB Article ID# PL8009817

Contents

SummaryDetails

Associated Components