NX Extract Body is creating individual features

2019-04-25T15:26:17Z
NX for Design

Summary


Details

--------------- 
When extracting faces, sometimes one feature is created and other times, 
several features are created. Why the difference?



Solution

 Using the Extract Body option Face Chain in the Face Option dropdown will 
create a single feature. Using Single Face will create multiple features.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1847
Function: FEATURE_MODEL

Ref: 001-7722224

KB Article ID# PL8009816

Contents

SummaryDetails

Associated Components

Modeling