NX Leader stub side preferences cannot be set in Annotation Preferences

2019-04-25T15:20:59Z
NX for Design

Summary


Details

--------------- 
Why is the Leader Side option always grayed out in Preferences --> Annotation 
--> Line/Arrow tab? How can you set the leader side when placing a label?



Solution

 By default, when creating dimensions, the leader side is inferred. If you do 
not want the leader side to be inferred, once the leader is rubberbanding, you 
can lock the leader side option to Left or Right by holding down the CTRL key.


The leader side option is only available in the Annotation Preferences dialog when 
editing multiple annotations. It was added in NX1 to make it easy for the user 
to edit multiple annotations.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1847
Function: ANNOTATION

Ref: 001-6886714

KB Article ID# PL8009806

Contents

SummaryDetails

Associated Components

Drafting