wrong nx launched from tc

2021-10-06T23:26:39Z

Summary


Details

  ) In a test environment, wrong version of NX launched from Teamcenter.
  ) Both NX 12, NX 11 are installed on the machine,
    but the older NX 11 keeps opening after double clicking a UGMASTER dataset.




Solution

  ) In Edit --> Options, user saw that this test environment had been setup
    for launching in multiple environments
  ) For example, the preference TC_NX_Environments had 2 values,
    corresponding to NX 11 and NX 12
    e.g.
      ENV11, ENV12
  ) Two TC_NX_Location preferences were found
    e.g.
      TC_NX_Location_for_ENV11
      TC_NX_Location_for_ENV12
  ) For this user, just had to set NX Environment in Edit --> User Setting ...
    to point to the desired NX 12.





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_OPEN

Ref: 002-8009798

KB Article ID# PL8009798

Contents

SummaryDetails

Associated Components