Using Teamcenter Information column to configure a different revision rule

2021-10-06T23:26:39Z

Summary


Details

Is it possible to get a list of updates to an assembly, thereby enabling the user to see which components they would like to update to a newer revision?




Solution

The TC Information column in the Assembly Navigator enables concurrent design among collaborating team members. It indicates in the current session if a newer version of a part is available in Teamcenter, or if a different revision of a part is available due to a different revision rule. You then decide whether to include the updates. 

To use the TC Information column with a different revision rule:
 
1) Set a revision rule in the Assembly Load Options dialog box and load the assembly. 

2) Set a new revision rule. 

3) Right-click on TC Information column and select Refresh Teamcenter Information . The TC Information column shows the new revisions/versions that are available, which is the difference between loading the assembly using the revision rule in step 1 and the revision rule in step 2. 

4) Choose File tab→Close→Close and Reopen Selected Parts . The Reopen Part dialog box is pre-populated with the newer revisions/versions that were reported in the TC Information column

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: ASSEMBLY_NAV

Ref: 002-8009792

KB Article ID# PL8009792

Contents

SummaryDetails

Associated Components