Solid Edge Solid Edge 2019 - Maintenance Pack 6 Announcement

2021-10-07T00:10:00Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

April 13, 2019
 
Dear Solid Edge Customer: 
 
Solid Edge 2019 Maintenance Pack 6 is now available for download.
 
Sincerely,
The Solid Edge Team 
 
============
Release Notes:
============
 
Solid Edge 2019 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
 
Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.
 
=====================
Maintenance Pack Version:
=====================
 
Solid Edge 2019 MP6
Version: 219.00.06.04
 
================
Download Location:
================
 
Solid Edge 2019 Maintenance Packs can be downloaded from:
 
   https://download.industrysoftware.automation.siemens.com/solid_edge/2019/Maintenance_Packs/
 
==========
Installation:
==========
 
  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
  • MSI Product Updates calculate free disk space before installing. Please be patient.
  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
  • Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
  • When uninstalling, the original source media must be available to allow the recovery of previous file versions.
  • The current MSI Product Update will be the only Update listed and available for uninstallation. 
  • After the current Product Update is uninstalled the previous Product Update will become the current Update.
  • .zip files delivered with this MP such as SEECAdministratorV219.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.
 
===============
E-mail Notification: 
===============
 
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
 
For details on initiating your email subscription navigate to: 
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html
 
============================================
This Maintenance Pack addresses the following PRs:
============================================
 
===General=== 
PR 9261665: Engineering reference, Gear design update problem
PR 9280124: Lower graphic card performance on "Tools" ribbon 
PR 9311226: Poor performance when checking out a floating license with options
 
===API===
PR 9398903: Parts being placed in the wrong position during reorder
 
===Assembly=== 
PR 9350209: Solid Edge is crashing while running route by part command
PR 9363289: Failed to extend/trim the highlighted frame component(s) using the selected tool
PR 9391936: Flickering when zooming in sketch edit in place in assembly
PR 9376223: Assembly File repair SE2019 MP4 request - SE is crashing after save attempt
PR 9402256: "SE Graphics Test 1" performance test is not running thru completion
PR 9405618: frames get messed up after updating
 
===Draft=== 
PR 9327095: Dimensions on a sketch disappear when you select a design object, and RMB show only
PR 8393282: added hole gets new hole number although size already exists
PR 8952766: User wants to skip 'define hole table origin' step during placement of new hole table
PR 9382515: Drawing View Wizard Option Crashes session
 
===Part/Sheet Metal===
PR 9173544: Problem with optimized geometry after optimize
PR 9291277: Save as flat DXF options unchecked " Complex Hole" gives wrong result
PR 9357495: Part file crashes while saving in sketch environment
PR 8389690: Region created from sketch with gap
PR 9352716: Move command, as part was moving to a distance double of the dragged distance
PR 9389334: Old generated closed corners cause failure in SE2019
PR 9325163: Abort when trying to move faces in Sync.env
PR 9397714: Construction body fails after linking the material in a design body part copy
PR 9403379: Solid Edge closes after editing pattern in assembly
 
===Translators===
PR 8551634: NX open the JT exported from SE, and the location of PMI dimension is wrong
PR 9304109: Unable to open SolidWorks file
PR 9343819: Not possible to open step file correctly parts missing
PR 9354990: Unable to save as DWG
 
===Data Management===
PR 9351345: Document controllers ignored, only first one can set data obsolete
 
===Teamcenter Integration for Solid Edge===
PR 9227116: LOV value will disappear when saving a new file
PR 9339858: Dynamic LOVs not working
PR 9343658: Teamcenter 12.1 Standard part ignores naming rule
PR 9342992: Assembly JT creation was very slow when wire harness is present
PR 9371297: Error on first Save to Teamcenter of drawing or assembly from active SE 2019 Part
PR 9375450: User must run the Replace Part command twice to successfully replace the part
PR 9383281: Solid edge is crashing randomly 
PR 9387708: AddToTeamcenter does not start import of the file if manifest file exists in the directory
PR 9240326: BOM line error with adjustable assembly
PR 9394831: Project removed when revise via Structure-Editor
 
===TechPub===
PR 9304665: Line Break in Illustration description not correct in HTML
PR 9330815: The "Isolate and Zoom" button cannot be activated in the PDF file
PR 9331438: 3D models are sometimes displayed incorrectly in the PDF file
PR 9355213: 3DPub and Illustrations: garbage square after FOA file name in model panel
 

SFB-SOLID_EDGE-8009788
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8009788

Contents

SummaryDetails

Associated Components

SE_BETA