The customer updated Solid Edge Fast Search from ST9 to ST10.
After this update the Where Used is not working anymore. After some
investigation the customer noticed that the SE* properties do not exist any
more on their vault location.
The customer tried to solve this by a manual registration of the
SEPropertyHandler.dll with the command:
regsvr32 SEPropertyHandler.dll
This command will fail with an error:
The module "SEPropertyHandler.dll" failed to load
Make sure the binary is stored at the specified path or debug it to check
for problems with the binary or dependent .DLL files
The specified module could not be found.
Solution
This is a Windows 2k8 server OS specific issue.
1. Uninstall the Fast Search setup if exists.
2. Use Windows update to install KB2999226
3. Restart the system
4. Install the Fast Search and it should work
Notes and References
https://www.microsoft.com/en-us/download/details.aspx?id=49077
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110.0
Function: SEDM
Ref: 001-8346692