In 'Pattern by Table':
What is the difference between 'Pattern origin point' (Quickbar) and the 'Parent reference point' (in table)?
Solution
Pattern Origin Point (on the Quickbar):
This allows the user to select a key point, other than the direction defining Coordinate system, as an origin for the pattern.
Selected Keypoint (in the Table):
Defines the reference point on the feature for the pattern. In other words, the values in the spreadsheet refer to this feature reference point relative to the origin point (Pattern Origin Point).
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V109MP6
Function: FEATURES
Ref: 001-8339602