Is Insight with SQL Server 2016 and Sharepoint Foundation 2010 supported?
Solution
No, because based on the Microsoft Software Requirements SQL 2014 and
accordingly SQL Server 2016 are not supported with Sharepoint Foundation
2010.
Visit the Microsoft Technet for details:
https://technet.microsoft.com/en-us/library/cc288751%28v=office.14%29.aspx#sect
ion4
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
> Software requirements:
Important
SharePoint Foundation 2010 is not supported on Microsoft SQL Server 2014.
Version support is determined by the equation in the following Note:
In order to maintain SharePoint and SQL Server compatibility we use the
"SharePoint N-1 on SQL Server N+1" equation to determine version support.
Using SharePoint Foundation 2010 as an example, the N release of SQL Server is
2008/2008 R2 and N+1 is SQL Server 2012. For Microsoft SharePoint Server 2013
the N release of SQL Server is 2012 and the N+1 is SQL Server 2014.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
From ST9 Implementation guide see the following configuration options
Win Server: 2008 R2;2012/2012R2
SQL Server: 2008 R2, 2012
SP Foundation: Search Server Express 2010 SP2
Sharepoint Server: 2010R2
or:
Win Server: 2012/2012R2
SQL Server: 2012 oder 2014
SP Foundation: 2013 SP1
Sharepoint Server: 2013 SP1
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 8.164
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109.0
Function: INSIGHT
Ref: 001-8313078