SEEC integration default item type

2021-10-06T23:54:56Z

Summary


Details

A customer has special Item type for SE Part and SE Sheetmetal files and 
another Item type for SE assemblies. However, you can only set one default Item 
type for a 3D file with the preference SEEC_Default_Item_Type.


Is it possible to add more Item types as default? Or is there another solution 
which would allow using more default Item types?



Solution

For a Solid Edge file, when the custom property "Teamcenter Item Type" is empty 
we will use the value in the Teamcenter preference SEEC_Default_Item_Type.  If 
that is missing, we will use the first value in the SEEC_ItemTypelist_* preference.


So the workaround for this issue is to add a custom property for the Item Type 
to the Solid Edge template file (the managed seed file).  This value will 
overwrite the SEEC_Default_Item_type and make it possible to set another 
default for a specific file type.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC

Ref: 001-7864475

KB Article ID# PL8009087

Contents

SummaryDetails

Associated Components