We are using Solid Edge with a Floating Simulation add-on.
The issue is that none of the users have access to Simulation.
Is there something wrong with the license file?
Solution
For a Floating Simulation add-on you need to turn it on for the Client.
Open Solid Edge with an assembly and under the Solid Edge Application button (top left) there should be an option 'Turn Simulation on/off'.
Notes
If you have further inquiries about Solid Edge Solid Edge Portfolio Products Licensing please refer to the FAQs Collection link below:
Solid Edge Portfolio Products Licensing FAQs Collection