Solid Edge Migrating drawings without parts from SolidWorks

2021-10-06T23:54:55Z
TRANSLATORS

Summary


Details

The user wants to migrate only drawings from SolidWorks - without parts and 
assemblies. Is this possible with the SolidWorks migration tools?



Solution

The 'Create Drawing Views on Migration' parameter in the SolidWorks2SE.ini file 
controls the creation of drawing views during migration. By default, the value 
is '1', which creates drawing views during migration.  Setting the value to '0' 
specifies that the option 'Export Drafts as PDF or DXF' is used rather than 
creating associative drawing views.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: TRANSLATORS
Function: SW

Ref: 001-8328633

KB Article ID# PL8009077

Contents

SummaryDetails

Associated Components

TRANSLATORS: OTHER