Can I use my cloud enabled Solid Edge when I end maintenance?

2021-10-06T23:54:50Z

Summary


Details

Can I still use my Solid Edge Cloud Enabled license when I end maintenance?



Solution

This is taken from a FAQ provided when Cloud was first released:


Q: When choosing the cloud option, can I still access my data if I'm not on maintenance or subscription? 

A. Yes. Your Solid edge data will be available to you after your perpetual maintenance or subscription has expires.


What is supposed to happen is if the user is out of maintenance, a warning message will pop-up. The machine the user is on at that time will become the only machine the Cloud License will work with. 


The license can only be used on one machine (the last machine that used the cloud license when in maintenance).

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Function: LICENSING

Ref: 001-8322948

KB Article ID# PL8009044

Contents

SummaryDetails

Associated Components