How do you check the interferences of all parts in an assembly?
Solution
This is same as checking for interferences of an assembly with itself. Do the following:
1. Click Inspect tab, Evaluate Group, Check Interference
2. For 'Select Set 1' simply click and drag a fence around the entire assembly
3. Before proceeding click 'Interference Options' button on the ribbon bar for the command,
4. Make sure 'Itself' option is selected for 'Check Select Set 1 against'
5. Click OK to dismiss the Options dialog
6. Click the 'Process' button on ribbonbar
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V109MP1
Function: TOOLS
Ref: 001-7854794