Installation SESP-Server initialize of SESP_Database failed

2021-10-06T23:54:48Z

Summary


Details

During a new ST9 Solid Edge for Sharepoint Server Installation and also on 
upgrading the server from ST8 the following message occurs and the SESP server 
Initialize fails:


SharePoint Content Databases Information 
The following permission(s) have not been granted to the "SESPUser" 
user on the 
1. "SESP_Database": 
 - Insert 
 - Select 
 - Update


Grant this permission(s) and then run "Initialize Solid Edge SP SQL 
Server" utility again.


Refer the Solid Edge SP Implementation Guide for more details.



Solution

We have here two issues - one for the upgrade and one for a new installation.


In case of upgrading from ST8 to ST9 the "SESP_User" must firstly be configured 
to the "SESP_Database":


1. Start Microsoft SQL Management Studio 
2. Expand Security and Logins 
3. Select sespuser with right Mouse button and open Properties 
4. Select User Mapping 
5. Look for SESP_Database and check the checkbox that the sespuser will be 
mapped 
=> result is Database:"SESP_Database"; User:"sespuser"; Default Schema:dbo 
6. Activate the Database role membership for: SESP_Database Area the 
"db_datareader" and "db_datawriter" by checking the checkbox 
7. Accept with OK


Now the following is for both cases - the manual activation of the needed 
permissions: 


NOTE: During a new ST9 Solid Edge for Sharepoint Server Installation the 
"SESPUser" is configured automatically to the "SESP_Database".


8. Expand Databases in the Microsoft SQL Management Studio 
9. Select SESP_Database with right Mouse click 
10. Open Properties 
=> The "sespuser" is listed in the User or Role Area 
11. Find and check each of the following: 
- Insert 
- Select 
- Update 
- Connect 
12. Accept with OK 
13. Run Initialize Solid Edge SP SQL Server


The Initialize should run now without any permission problems.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109.0
Function: SESP-WEB

Ref: 001-7785776

KB Article ID# PL8009030

Contents

SummaryDetails

Associated Components