Solid Edge Solid Edge - Sharpness set default setting

2021-10-06T23:54:48Z
PART/SHEETMETAL

Summary


Details

In View -> Style group is it possible to set the 'sharpness set' to a higher default level than 2?



Solution

In the 'View' section of the Solid Edge options there are two settings - an 'Auto-sharpen' command that is off by default and the Arc smoothness command. 


The setting for 'Auto-sharpen' is remembered.


This should do the trick for you regarding View quality but remember that this affects the View Performance.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: PROFILE/SKETCH
Version: V109.0
Function: DISPLAY

Ref: 001-7879901

KB Article ID# PL8009025

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES